Other Parts Discussed in Thread: DRV8833, DRV8813, DRV8872,
Our customer has a question about Motor driver ICs.
I'm posting the question for the customer:
When in Sleep Mode, are the nFAULT outputs of the following ICs valid?
(1) DRV8881E
(2) DRV8833
(3) DRV8813
(4) DRV8872
I'd like to check the below;
There is the following explanation of UVLO in DRV8881 datasheet;
"If 'at any time' the voltage on the VM pin falls below the undervoltage-lockout threshold voltage,
... the nFAULT pin will be driven low. "
Does the 'at any time' include time which is in SLEEP mode?
Thank you in advance.
Best regards,
Takishin