This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8833: Can it work well with 3s Li-ion battery(3.7V×3)?

Part Number: DRV8833

Hi:

I’m dong a project with DRV8833 to drive 2 motor. I notice that the voltage range is form 2.7V to 10.8V. If i use 3s Li-ion (3.7V*3),is it safe?

Thanks,

Wang