The DRV10983 is such a nice part, but I need to control a brushless, sensorless motor with 24V@60A/Phase. I was thinking of simply adding an H-bridge FET driver to each output and using that to drive some large FETs. Secondarily, it would be very nice (but not mandatory) if the circuit could do regenerative braking. Can this part be made to work, or is there a better solution?