Hi,
I'd like to know in which state are the mosfet gate drive outputs on the DRV8301 during dead-time.
On the oscillograms I've recorded, it seems to be an open drain output, please would you mind confirming this?
Thank you
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'd like to know in which state are the mosfet gate drive outputs on the DRV8301 during dead-time.
On the oscillograms I've recorded, it seems to be an open drain output, please would you mind confirming this?
Thank you
Best regards
Hi Rick,
thank you for your answer.
I thought it was the way you write it above, however as I try to understand the oscillograms, it seems that Vg signal doesn't go to 0V before the end of the dead-time.
And so for a short time duration (around 100ns at ton and toff), there is a shoot-through between the high-side MOSFET and the low-side one.
Please see the oscillograms in attached files.
Channel 1 (yellow) is the high-side Vg signal, Channel 2 (blue) is the low-side one.
My interpretation : when Vg (high-side MOS) goes low, the bootstrap capacitor (100nF) takes too much time to discharge (around 500ns).
And when Vg (low-side MOS) goes low, I think the filter capacitors (C64, C67, C70, 1nF) on Rshunts are too high and create a long delay that prevents the voltage to go down fast.
Also, I think I always had this problem, but before I had 10 ohms gate resistor values (please see the extract schematics in attached files) for R144/145, R147/148 and R154/155 so the shoot-through duration was really low (around 10ns).
Now, for EMC reasons, I need to have higher gate resistor value, eg 82 ohms, so shoot-through duration is higher and the MOSFETs get warmer and warmer.
Do you think I could lower the value of bootstrap capacitors and Rshunt filter capacitors?
Thank you,
Best regards
Hi Alexandre,
Have you tried adjusting the DTC resistor or increasing the dead time via the mcu?
When increasing the gate resistor, the driver can interpret the FET as off before it actually is.