This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8871: Continuous Current Rating

Part Number: DRV8871

Hi,

What is the continuous current provided by the DRV8871 motor driver? I understand that it's peak current is 3.6 A (I assume this is only for a few milliseconds) but I'm confused as to what the current output is under normal/recommended operating conditions or what the driver can sustain for longer periods of time. For reference, I would like to use the driver with a 10 W, 9 V motor and I'm trying to ensure that the driver can provide the necessary current to run the motor for extended periods of time. Any help would be appreciated.

Thanks,

Rachel