This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8320: Fault Action and Response of the OCP Setting by Hardware Version

Part Number: DRV8320

My customer is interested in the DRV8320H with hardward interface. But we don't see the setting on the Datasheet's Table 7. it looks they are for the SPI interface,not H/W interface right?

how to setting the Fault Action and Response as Table 7 with H/W interface?

Regards,

Brian

  • Hi Brian,

    Table 7 applies to both SPI and Hardware devices, but needs some clarification.

    Some modes listed in Table 7 are only available in the SPI mode. An example is OCP_MODE. All four modes are available in the SPI version. Only two modes are available in the Hardware version (retry and disabled).