This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8824EVM: DRV8824 EVB application question

Part Number: DRV8824EVM
Other Parts Discussed in Thread: DRV8824

Hi Sir 

drv8824 nRESET  pin always low when we connect EVB and press " connect"? is it normal? (output we have no connect to motor)

any set up we need notice? or we can direct pull this pin to hign?

drv8824.docx 

  • Hi Chen Bogey8,

    Once the EVM is connected, please try:
    1) left click the Reset box in the Motor Control area or
    2) left click the nRESET pin

    Does the nRESET pin change to green or red?

    If it does not, please confirm the COM port selected in the pulldown is correct.