Hi,
I am trying to drive a motor I designed with the DRV10983EVM board, and I am struggling to get it to work properly.
Summary:
1. We managed to drive the motor in open loop control. However when the closed loop control is enabled, the motor always drive up to the open to closed loop threshold and then stops. The sin current waveform of constant amplitude dies to zero rapidly. In the display panel of the GUI, the Lock indicator will be on and the motor restarts and repeat the same process a few seconds later.
2. I tried to adjust the transition threshold from low (a few Hz) to high (204 Hz), not much difference.
3. At 204 Hz, my motor should give a 1.4 peak back emf. Is it large enough for the Drive to detect?
Any suggestions?
Ning