Hi this is David!
I am currently developing motor driver board with ti's drv8323rs chip(btw, I love this chip xD)
Anyways, I am using 1x PWM mode and there's a problem with this.
Whenever I put ENABLE to high it goes back to the initial value which is 6x PWM mode.(which is normal operation)
The problem here I think here is that the hall sensor line goes directly into INLA, INHB, INLB and do something with 6x PWM mode(might short since hall sensor INHB, INLB can get high on the same time)
So the motor makes some quite a loud noise before I turn into 1x PWM mode through SPI.(sometimes so large amount of current go through even the battery BMS cut the power)..
is it a defect?
if not, how can I solve this problem
Thank you for your help