Other Parts Discussed in Thread: DRV8304
Hello All
Currently working on a new design using the DRV8303, but I don't want to use leg shunt resistors. I want to tie all the low side source's of the fets together and have one shunt for all 3 legs.
Now, as the voltage coming off the shunts will be positive and i want as high resolution as possible. Please can you confirm it is ok for me to do the following...
- Tie Vref to GND
- invert the inputs SN and SP so that SN connects to the GND and SP connects to the low side source's.
So this makes a non-inverting opamp that should give me an output between 0 (GND) and AVDD that is directly proportional to the load through the shunt. The different gains should remain adjustable via the SPI.
Please can you confirm this is all OK before I finish off the schematic?
Thanks