Hi all,
I have questions about the PHASE control of DV8801-Q1 as below;
(1) If CW / CCW switching is performed by PHASE signal while ENABLE = "H",
Is there a problem with the drive stage or IC?
(2) Is it necessary to change CW / CCW while ENABLE = "L"?
If yes,
Is it necessary to confirm the motor stop?
Under what conditions can you change PHASE even if you keep ENABLE = "1"?
【Motor specification】: DC brush motor
· Rated voltage: 24 VDC
· Rated load: 9.8 mNm
· Rated power consumption: 1.4 W
* Actually, it is used at DC 20 V, and the steady current value is 250 ~ 350 mA.
Best regards,
Toshi