This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: Auto offset Calibration

Part Number: DRV8323


Hi,

The DRV8323/DRV8323R devices can perform an automatic offset calibration through the SPI registers or CAL pin.

I want to use the calibration through the SPI register. Which state of the pin CAL ? Not connect, tied to GND, tied to 3.3V ?

Thanks,

Mikaël