This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10987: inductor for the SW pin of DRV10987

Part Number: DRV10987

hi,

i use the part DRV10987 as a driver to a circle motor. i got from the WEBENCH tool that in the SW pin i need to insert an inductor of 47uH. I dont have many space in the board. need the smallest inductor that fits.

which inductor do tou recomend? 

Maximum DC Current:1 A
the drv10987 voltage output is 30v.
thanks,
Liraz Abramovsky.