hello
I have to put some thought on how to test a DRV10983 over a range of bldc motors parameters
I could use different bldc motors for each test; but is it possible to test a DRV10983 against another DRV10983?
I would isolate them with a transformer, seems the DRV10983 can absorb some power, with a correct circuit design
do you think this is feasible?
also
does TI have a C source code file for the DRV10983 with the registers (something like DRV10983.h)
I've written one but would like to have different sources if possible
regards
enzo