This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8305EVM: How to enable BOOSTXL-DRV8305 mosfets for switching via LaunchXL-F28379D

Part Number: BOOSTXL-DRV8305EVM

Hello,

I am trying to control the booster pack, programming the launchpad via Matlab's Embedded Coder Support Package for Texas Instruments C2000 Processors (version 17.1.6).

I have implemented a control loop for the output current, and when trying to test it, I get 0 A in the output.

Before sending any command, I am setting the DriveEnable signal to 1.

The problem is that when I send the PWM signals to the booster pack this does not seem to respond, as no switchings happen in the phase outputs.

The booster pack has all the power supplies at their correct levels, and the PVDD is set to 24 V.

Am I not sending some signal that enables the switchin of the mosfets?

Thank you,

Imanol