This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L: Use the driver without EN pin

Part Number: DRV2605L


Hi!

My plan is to drive an ERM (eccentric rotation motor) with the DRV2605L. My application requires me to minimize the number of connections I use.

Can I use the driver by always pulling up the EN pin and using the standby mode for low consumption via I2C ?

  • Hi Karim,

    Welcome to e2e.
    Yes, that's something you can do to minimize the control signals in your application.
    You can use Register 0x01, bit 7 to reset the device and take it into a known state, if needed.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators