This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10987: Improvements wished

Part Number: DRV10987


I don't know if this forum is the good place to formulate wishes.

The DRV10987 is mainly intended to rotate miscelaneous fans in the home area (pedestal fans,...).

However this little device can be found very convenient to control small BLDC motors in the mechatronics area.

In this case, two improvements would be very useful to get full control of a motor via the I2C port:

- The possibility to control the direction of rotation via the I2C port (1 bit in the 0x30 register ?)

- The possibility to maintain the device out of the standby mode when the speed register is assigned to zero, and thus avoid the long 350 ms delay to drive motor after exiting standby mode. One bit would be sufficient in a CONFIG register.

Froggy