A customer I support is looking for a driver that can drive solenoids from 5 to 24V @ 100mA (200mA current limit).
Since the DRV120 is an open drain driver, is it OK to power the device itself from a voltage rail that is within the datasheet specs (6V-26V) and have the solenoid connected between a 5V - 24V supply and the open drain output?
If the customer does not want to use the hold current option, can he connect the KEEP pin to ground, thereby keeping the device operating on the peak current setting? Is then the PWM dutycycle 100% (continuous ON)?
I assume that the PWM operation only kicks in when the HOLD mode is active , PWM dutycycle determined by the R-hold setting? Pls. comment.