Hello all,
I am trying to control a 24V DC motor using DRV8871 breakout board from Adafruit . I got into this situation I can't quite explain.
The motor runs fine if I hook it up directly to 24V Power Supply. I am using 24V/2.5A MeanWell Power Supply. .
However, when I control the motor through the breakout board, the output voltage is only about 5V. The PWM frequency I used to control the motor is 60HZ at 75% Duty Cycle. I tried to change the resistor to a lower value in order to allow more current pass through if needed, it doesn't change the situation. I also monitor the current pull by the motor, it drew around 0.5 A no load and around 1 A with load, that means the Power supply has plenty of current to run the motor, I believe.
Please help me explain this situation, if possible, do you have any idea how to fix it?
Thanks,
Alex