This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8701: In possible to set VREF at 5V

Part Number: DRV8701


Hello,

I have the DRV8701EVM and the maximum VREF is 3,3V. I see the datasheet of the DRV8701 and it indicates that we could set VREF to AVDD (5.2V max).

I understand that the maximum for the DRV8701EVM is setted to 3.3V for protecting the develop board. If I develop a new board for motor control I could set the VREF to AVDD to obtain high level currents?

Thanks a lot.