Hi all
Would you mind if we ask DRV8301?
<Question1>
Is it possible to communicate using SPI(Read and Write) with follow condition?
Condition : PVDD1=OFF(0V), VDD_SPV=ON(+5V), EN_GATE=High
<Question2>
After writing resister using follow CondtionA, Power condition changes from ConditionA to ConditionB.
In this case, does DRV8301 keep register data which are wrote with ConditionA?
ConditionA : PVDD1=ON(+24V), VDD_SPV=ON(+5V), EN_GATE=High
ConditionB : PVDD1=OFF(0V), VDD_SPV=ON(+5V), EN_GATE=High
Kind regards,
Hirotaka Matsumoto