Hi,
I'm using DRV8701E to to driver 12V BDC motor, when set forward mode via EN/PH, the nFault pin is low at the time.
but the VCP and AVDD, DVDD are generated well. after check datasheet, it should not UVLO on VM(+12V) and VCP (21.6V);
we can AVDD=4.8V, DVDD=3.3V already. we set IDRIVE into 25/50mA mode.
but the motor has doen't work.
Vds =12V all the time. don't know how to let motor work. i paste my circuit here.
Any ideas?
Best Regards!
Orin