This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single-phase Full-Wave Fan with hall element for Automotive application

Other Parts Discussed in Thread: DRV8702-Q1, DRV8702D-Q1, DRV8703D-Q1, DRV8703-Q1, DRV8701, TIDA-00875

We're looking for pre-driver with single hall element application for single-phase Full-Wave fan.

Min Input voltage: 4.5V (System voltage: 5V, 12V and 24V)

Used hall elements: Niceri520/Niceri524 or AKM solution

Control requirements: Speed Closed loop

Comptitions: LB11850 or Apx9211

Customer: WW class fan maker

Is there any similar solution? Or any suggestions on this application? Very thanks.

Regards,

Brian