This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8301: IICDC2017 : Query regarding DRV8301 booster pack

Part Number: BOOSTXL-DRV8301
Other Parts Discussed in Thread: DRV8301

Respected Sir/Madam,

        Is it safe to drive a BLDC motor with following specifications using the DRV8301 Booster pack (BOOSTXL-DRV8301) and C2000 F28069M piccolo launchpad (LAUNCHXL-F28069M)

PEAK CURRENT : 18A

RATED CURRENT : 10A

VOLTAGE : 24V

 Thank you

Regards,

Vignesh.J