Hi,
I'm seeing an issue where the DRV8308 nLock pin is reporting lock (low), but if I load the motor and monitor FGout, FGout will stretch. This is in Clock Frequency Mode, speed is set to 300 and at a frequency of 50Hz, which translates to 750RPM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm seeing an issue where the DRV8308 nLock pin is reporting lock (low), but if I load the motor and monitor FGout, FGout will stretch. This is in Clock Frequency Mode, speed is set to 300 and at a frequency of 50Hz, which translates to 750RPM.
Hi Rob,
Are you evaluating this functionality on our DRV8308EVM? Did you follow the steps for tuning Clock Frequency Mode from our User Guide? There are some filters and other features that need to be tuned for Clock Frequency Mode to work well.