I am interfacing TMS320F28335ZHHA to DRV8312. As the AGND and GND are separated only via a resistor, do I need to connect any opto isolator to the pwm input to the drive or I can directly interface the PWM channel of the controller to the drv8312?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am interfacing TMS320F28335ZHHA to DRV8312. As the AGND and GND are separated only via a resistor, do I need to connect any opto isolator to the pwm input to the drive or I can directly interface the PWM channel of the controller to the drv8312?