Part Number: DRV8323
Other Parts Discussed in Thread: MSP430F5529, DRV832X,
Hi,
a customer is using the DRV8323BOOST boosterpack with the MSP430F5529 LP are able to run the OOB Trapezoidal Sensored and Sensorless BLDC from the DRV832x_EVM_BLDC_FW_1.0.0 package.
The DRV8323 mentions sinusoidal commutation as well.
Are there any examples for sinusoidal commutation available, even if it is on a different MCU like C2000?
I noticed there is an Instaspin FOC example with C2000, but here we would need just a Hall sensored BLDC control, but with sinusoidal commutation.
Thanks,
--Gunter