Hello,
Our customer check the P16 on the datasheet.
It is estimated the RDSon as 0.72ohm at Ta=58 degree.
How did you estimate this value?
Refer to the Figure 1, the normalized RDS0n is 1.18 at Ta=58 degree.
The RDSon is 0.565 ohm typ, 0.68 ohm max. So, at Ta=58 degree, it is from 0.666 ohm to 0.802 ohm.
Best Regards,
Naoki Aoyama