Hello,
My customer is using the DRV8824 motor driver in a 34V application. The motor outputs, AOUT1, AOUT2 and BOUT1, BOUT2 are all connected to a 4 pin connector straight from the driver. The motor then gets plugged into this connector.
The customer is conducting +8kV contact ESD testing on the connector and finding that the DRV8824 are getting damaged. They have tried to fit separately 43V SMA TVS diodes from each of the 4 pins (AOUT1 AOUT2 etc) to ground.
When the diodes are bi-directional ones (SMAJ43) they are not effective and the DRV8824 still fails. When the diodes are unidirectional (SMAJ43A) , it went through the entire test without failure but there were some driver lockouts after some hits. They also observed decay current going through the unidirectional diodes.
They need help to solve the ESD problem for their system and would like to hear all ideas plus an explanation why unidirectional diodes may affect the operation (during decay).
Thanks very much
Faizul Bacchus