Hi,
I am considering the DRV8412 as a TEC driver for a TEC that operates at 24V and can draw up to 4A. In parallel mode I believe the DRV8412 should be more than adequate for this combination of PVDD and current, correct? Or is there a derating of the output current in parallel mode that scales with the value of PVDD? For example, if the maximum output current is 6A at 12V, does this value drop to 4A (or less) at 24V?
Regards,
James