Other Parts Discussed in Thread: DRV2700
Hi Folks,
I want to use DRV2700EVM in following setup:
- VIN supply: J2 @ 3V3 and JP10, JP11 set to VIN
- Single ended input (connect regulated voltage supply 0V to 3V3 @ TP7 +, TP8 GND)
- Single ended output with TDK PowerHap 2.5G Piezo connected to Out+ / GND
- No MSP interaction: Jumpers JP5,JP5 open
- BST set to 83V
- GAIN: Diffent gains tested
- JP12 is set
When Piezo is connected there is loud accoustic noise from Piezo, the output voltage drops to 0V with spikes /Audio frequency). Another Piezo would not work either.
When I remove the Piezo and measure output voltage there is an gain depended offset voltage of e.g. 40V @ 40.7dB. Increasing input voltage slowly from 0V to 3V3 will partially work: The voltage range from 40V to 83V works as expected :-)
I wonder if I miss something ? Or what I did wrong ?
Any suggestions ?
BR
Niels