Hello,
I'm trying to use DRV8803 Motor Driver
but, I think that I have to check first below functions are possible by DRV8803
1. is it possible that I can controll Bipolar Stepper Motor by DRV 8803?
Cause, Datasheet only mentions about Unipolar Stepper Motor Drivers on first Page
2. Also, I want to use 1/8 Microstep Controll by DRV8803. is it possible?
3. I heard that Unipolar Stepper Motor cannot rotate reverse way.
and since the DRV 8803 datasheet only mentions about unipoar stepper Motor,
is it Still Possible that I can controll my Bipolar Stepper Motor by DRV8803, in both way (forward and reverse) ?
thank you!