Other Parts Discussed in Thread: DRV8873
Hi team,
There is a case that the DRV8873 does not operate when VM turns on with low voltage setting.
We want to use that VM is 5V.
Although it does not operate when VM is started at 5V, it operates at 5.1V.
DRV8873 is active even if VM is started up at 6V and gradually lowered to 5V or less.
There seems to be a threshold in the vicinity of 5V and it seems that it will not begin to operate unless the VM once exceeds this threshold.
Are there restrictions on startup in this device or this EVM?
Best regards,
Tomoaki Yoshida