This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8301: Compatible with LAUNCHXL-F28069M?

Part Number: BOOSTXL-DRV8301
Other Parts Discussed in Thread: LAUNCHXL-F28027F, LAUNCHXL-F28069M,

Hi all, 

I am fairly sure from reading online that all the BOOSTXL booster packs are compatible with any of the LaunchXL LaunchPads, but I just wanted to triple check before purchasing. 

Will the BoostXL-DRV8301 be physically compatible (ie: pin connections) with a LAUNCHXL-F28069M? Having read the BoostXL-DRV8301 manual it mentions "Combine with compatible LaunchPad XL kits to create a complete 3-phase motor drive control platform" and then says it is optimised for the "LAUNCHXL-F28027F LaunchPad" so I wanted to confirm as this wording was a little confusing for me as it never mentions if it is compatible with ALL LaunchPads. 

Thank you kindly,
Matt