This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8837C: OCP in start up

Guru 16770 points
Part Number: DRV8837C
Other Parts Discussed in Thread: DRV8848

Hi

Is it valid OCP function when the motor starts up?

We require 1A output constantly, but 3A may be required when start up. 

Can we use DRV8837C?

BestRegards