This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8803: DRV8803

Part Number: DRV8803

Dear Sir,

We are using the IC DRV8803. We are driving the RESET pin from our system with 3.3V logic.

We would like to know the operating voltage range for the RESET pin. Since this detail is not available in Datasheet

  • Hi Giresh,

    The RESET pin operating range is 0 to 5.5V. Using 3.3V logic will work.

    Some of the information can be found be searching "Digital input pin voltage" and "Logic-Level inputs".