This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
Use the stepper motor driver chip DRV8825, use the mixed attenuation, the current is set to 2, 2A, drive a 1.5A stepper motor, use 24V voltage. As long as it is enabled, the motor will squeak, and if the CLK signal is sent, the motor will shake violently and the whistling sound will increase.
Hi Eric,
what's the sound of squeak? stepper motor can make sound by itself.
can you provide the motor information?if the step frequency is equal the motor natural frequency,motor will shake violently, you can change the microstep to decrease shake.
Thanks.