Other Parts Discussed in Thread: USB2ANY
if i configure the motor parameters in one time using usb2any explorer. After that can i run the motor without using usb2any exlporer is it possible??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
if i configure the motor parameters in one time using usb2any explorer. After that can i run the motor without using usb2any exlporer is it possible??
Hello deva kumari,
The USB2ANY translates the USB protocol to I2C protocol to communicate with our device. Usually the USB2ANY explorer is used to update the firmware of the USB2ANY. As a result, I assume you're asking if it is possible to control the motor without the USB2ANY.
Yes, the motor can be run without the use of the USB2ANY. Settings for the driver can be programmed into the EEPROM and an Analog or PWM command on the SPEED pin can control the speed.
I'll answer how to program the EEPROM in your other post.
Best,
-Cole