I ideally would like to GND the themal pad under this IC as I need it to be able to link a GND plane, in the datasheet it states that it has to be connected to the PCB (of course) but it does not state if it can / should also be connected to GND. My assumption is that it can be optionaly connected to GND but it would be great if some could confirm? Thanks Chris