Other Parts Discussed in Thread: DRV10987
Hello all !
I installed the GUI software to be able to communicate with my DRV10987 EVM Board.
The phase resistance parameter of my motor is 1,5 ohms.
When I try to enter "1,5" into the box, the software records "2".
The dot "." is not accepted.
When I try to enter "1500m" (I know that the GUI software has been developped with LabView ;o) ), I can quickly see "1,5" and then the famous "2" appears again.
I think this is related to the fact that I enter my values with a french keyboard (I'm from France), but I made a try with an american keyboard (qwerty) and an other try by setting my windows environment to english U.S.A. Nothing/Nada/Rien !!
Do other people cannot enter floating point values for this parameter in this Software ?
This is huggely disappointing because I have a phase resistance of 1,5 and not 2 ;o)
Thank you in advance for giving me an advice/trick/solution, because everything else works well and the DRV10987 is a very very good component !
Marco