Hello,
I am looking for recommendations on valve driver boards that can control 128 valves. Does TI manufacture driver boards for such applications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am looking for recommendations on valve driver boards that can control 128 valves. Does TI manufacture driver boards for such applications?
Hi Sarvesh,
While we have 7 channel devices like the TPL7407LA and ULN2003A for driving inductive loads such as valves, we do not have boards designed for driving large amounts of valves.
Thanks,
Alek Kaknevicius
Hi Sarvesh,
Do you mean each valve requires up to 1A? The DRV8860 can only provide up to 560mA unless you parallel the outputs per figure 6 of the datasheet. Also please note the current output graph is is at 25C, so the values will be reduced as the temperature increases.
For 1A for each valve, the DRV8806 may be a better option. There is a DRV8806EVM available also.