Other Parts Discussed in Thread: INSTASPIN-BLDC, DRV8301, CONTROLSUITE, DRV8302,
Hello,
I spent many hours trying to spin my motor with very little success.
I am focusing on "PWM control mode"
#1:
The only way I can keep the motor spinning is to enable "Advanced Startup Options"
but even with this enabled, the control seems to stay in "Startup" mode (the main Knob=duty cycle has no effect).
The main knob only affects the spinning direction (CW or CCW) but has no effect on RPM
#2: The BEMF waveform (Vag = Second graph: Displays the PU Phase-A BEMF waveform) seems strange:
I am using
InstaSPIN-BLDC_GUI_DRV83xx_v104.exe
+
InstaSPIN-BLDC_GUI_DRV8301_v104.out (reflashing the MCU with this did not change the behavior)
Can you help?
Thanks.