Other Parts Discussed in Thread: DRV10983, DRV10983-Q1
Hi TI support team.
When I was developing with DRV10983, I had a good advice from Cole.
Now I'm dong with DRV10983Q1 and had a almost same problem, but it does not same problem.
I have succeeded in driving a motor with DRV10983Q1 in my board. ISD, IPD are all enabled and motor speed is controlled by I2C speed command.
But 3~4 % of testing sample has a problem almost same as before when I use DRV10983, but this time VREG is flat 5.0V
When this occurs, even IPD did not work (there was no IPD sound).
In this case, if I move the motor slightly with my hand, the motor starts to rotate normally. (still there is no IPD sound)
It was a symptom that did not appear at first, but it continues to occur in many target boards.
Below is the register value when above happens.
0x0 0x1
0x1 0xa
0x2 0x86a0
0x3 0x1da2
0x4 0x3ff
0x5 0xd0
0x6 0xb348
0x7 0x0
0x8 0x102
0x30 0x8167
0x31 0xc0de
0x32 0x1
0x33 0x0
0x34 0x0
0x35 0x0
0x36 0x0
0x90 0x6e9
0x91 0x3f2a
0x92 0xe85f
0x93 0x2a97
0x94 0x3e4f
0x95 0xbd3f
0x96 0xc6a
And below is the register value when it operate normally
0x0 0x1
0x1 0x510
0x2 0x31c
0x3 0xe7
0x4 0x42d
0x5 0xd0
0x6 0xa6a6
0x7 0x0
0x8 0x102
0x30 0x814d
0x31 0xc0de
0x32 0x1
0x33 0x0
0x34 0x0
0x35 0x0
0x36 0x0
0x90 0x6e9
0x91 0x3f2a
0x92 0xe85f
0x93 0x2a97
0x94 0x3e4f
0x95 0xbd3f
0x96 0xc6a
One more strange thing is the fault code. There is no over current in my board but fault code always (except no motor rotation) 0x01
Did I miss anything?
Regards,
Peter