Hello,
If we want to pass EFT/Burst tests do we need to put extra TVS diodes on the motor phases(Outputs of DRV8313)?
What is the proper TVS diode then? I can't find proper TVS diode suitable for 48V motor and clamps 65V.
Do we need to pass this standard tests when motor and driver are close to each other with short cables ? which protections should be considered with this chip?
Thanks in advance.