Hi,
I need an Auto grade 3-phase bldc motor MOSFET driver IC. The IC should be hardware configurable, should not have interface like SPI.
I got a part from TI (DRV8320H), which is hardware configurable but not Auto grade. Can anyone help if i can get this part with automotive qualification.
Or if there is any other part without SPI interface and Auto grage?