This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312: Leackage current of the DRV8312

Part Number: DRV8312

Hello

 

We are using the DRV8312. In my board, the DRV8312 supply voltage is 12V, and the motor supply voltage is 24V.

I see that if I power the DRV8312 (turn on the 12V), and do not power on the 24V, I can see a voltage of 6.5V on the motor supply.

When activating the motor supply I do not see the 6.5V voltage, and I see the 24V OK.

 

Can there be some kind of leakage through the DRV8312?

 

regards

Oded