the specification is listed below:
DC MOTOR
Can control the speed using pulse width
motor driving voltage:28V
current should not exceed 1.25A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
thank you Matt suggesting.
could please suggest me a single IC driving more than 2 motor, with higher amperage.