This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8302: DRV8302

Part Number: DRV8302
Other Parts Discussed in Thread: DRV8320, DRV8323, DRV8308

Do you have a controller like DRV8302 but has a speed control closed loop ? Liked the capabilities but need the TACHO hall output and a PWM input. Liked the 60V, since there are 47V and 80V line transient pulse requirements.

  • Hi Les,

    Have you looked at the DRV8320, DRV8323, and DRV8308?

    The DRV8308 has a speed control closed loop, but lower voltage. The DRV8308 requires hall sensors to operate.
    The DRV8320 and DRV8323 have higher voltage, and 1x/3x/6x PWM mode. If operating in 1x PWM mode, hall sensors are required.