Hi guys,
i have a question regarding the DRV10987 spread spectrum modulation control functionality.
According to the datasheet, one can set the CONFIG1 Register Bit 15:14 for spread spectrum modulation control as follows:
00: No spread spectrum
01: ±5% dithering
10: ±10% dithering
11: ±15% dithering
For testing, i have attached a current probe into one motor phase, connected it to a spectrum analyzer and captured the following screenshot
- No SSM -> green trace
- 15 % dithering -> yellow trace (Similar results can be seen with ±5% dithering and ±10% dithering.)
PWM freq was set to 50 kHz. One can clearly see the peak and its harmonics. However, I would have expected the peaks to more or less disappear and the overall noise level to rise when enabling the SSM.
Any suggestions? Am i doing something wrong? To me, it looks like the PWM frequency is shifted but not increased regarding the bandwidth.
Help is highly appreciated.
Thanks in advance, Jonathan