This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2603EVM-CT: Control the strength of vibration by DRV2603

Part Number: DRV2603EVM-CT
Other Parts Discussed in Thread: DRV2603

Hi. I want to make 3 levels of vibration on the device (low, middle, high), so can I control the strength of vibration with DRV2603 by changing the PWM duty cycle?

  • Hi Anar,

    That's correct. Changing the duty cycle will change the vibration strength, this is according to figures 11 and 12 from data sheet depending on the actuator (LRA or ERM).

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators